11/21/2019 4:07 PM | |
Joined: 11/21/2019 Last visit: 1/25/2023 Posts: 6 Rating: (0) |
Hi everyone! I have new project, where I must to connect PLC S7-1512SP and SIPROTEC5 relay (7UM85) through PROFINET. My configuring based on manual "SIP5_ComProt_V07.80_Manual_C055-4" and https://support.industry.siemens.com/cs/ww/en/view/109743292. See attachments siprotec5: 7UM85-DAAA-AA0-0AAAA0-AQ0121-A3311B-AAA000-000AC0-CH2BA1-CB2 Connected PLC S7 1512SP (RJ45 connector, Profinet port) to SIPROTEC5 (RJ45 connector, CH1 module ETH-BA-2EL) Select the following measured values, which contain some values on the SIPROTEC screen: - Network frequency f - Voltage AB - Power active summed Psum These parameters are configured for SIPROTEC via DIGSI in the section "Communication distribution", supplied by X and input No. (1, 2, 3). On the other side, SIPROTEC appeared in the PLC downloaded to the GSDML project file . Inserted, plugged, dropped into its configuration just in case 2 blocks of 6 records (Measured values06). Addresses appear in the address space to view the function specified in the application: L PID x T DB10.DBD y, etc. (Taken from the manual, p231.) Also tried connections in the gap J, but the result is the same.. After 5 days result is 0.. Data not recieved in PLC. I ask for your help Thank you and have a nice day! Attachmentsiprotec5 & S7-1512SP.zip (227 Downloads) |
Last edited by: Jen_Moderator at: 11/22/2019 12:44:20Optimized link. |
|