3/12/2015 1:54 AM | |
Joined: 1/25/2015 Last visit: 4/21/2022 Posts: 22 Rating:
|
Dear Expert,
- Actions details In 315f-2pn / dp programming (complete actions) See attached screenshots In 1516f-3pn / dp programming (not complete actions) See attached screenshots In 1516f-3pn / dp programming (modified to complete actions) See attached screenshots it seems to When program scan, last status of data is not circulation. - What I want to know 1. S-1500 CPU and S300 scan type different from the program scan type in CPU? 2. If the program is different scan type, the scanning system setting possible on the CPU settings?
Attachmentscreenshots.zip (708 Downloads) |
Follow us on