4/29/2013 11:12 AM | |
Joined: 8/9/2011 Last visit: 11/1/2023 Posts: 324 Rating: (19) |
Hellow All After I upload the PLC Program to my Laptop i get most of the PLC tags showing ambiguity even though i dont find any two tags sharing the same address. Also 1) All of my tags get grouped into the default tag table leaving the other tag tables empty.!!(printscreens Before & After) 2 )Tag Always on has this problem but not the tag first scan even if they belong to the same system byte(last 2 princseens) Machine runs safely Thanks After rewiring the tag that yellow colour for the tag goes off!!! but i cant rewire those lakhs of tags (SP2)
AttachmentNew Microsoft Excel Worksheet.zip (319 Downloads) |
Last edited by: GAJENDRADS at: 4/30/2013 8:47 AMLast edited by: GAJENDRADS at: 4/30/2013 8:44 AM"Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
4/30/2013 4:59 PM | |
Posts: 267 Rating: (24) |
Hello, how do you upload the program from the PLC? In my STEP 7 V11 the upload button is always grey for a S7-1200. |
4/30/2013 5:35 PM | |
Joined: 1/28/2009 Last visit: 1/19/2025 Posts: 6858 Rating: (1366) |
Hello, Have you tried procedure here: Using the "unspecified CPU" to upload the hardware configuration and also: How upload a S7-1200 program in STEP 7 V11 SP2Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 4/30/2013 6:12 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on