5/22/2021 7:09 AM | |
Joined: 12/18/2014 Last visit: 7/21/2024 Posts: 33381 Rating: (4143)
|
So you want a scaling from -1,00 to 39,00 bar? What is the output of the transmitter? 0-10V? Or 0/4-20 mA? |
5/22/2021 12:22 PM | |
Joined: 5/17/2021 Last visit: 3/23/2022 Posts: 8 Rating: (0) |
0-10 v sir |
5/25/2021 8:07 AM | |
Joined: 5/17/2021 Last visit: 3/23/2022 Posts: 8 Rating: (0) |
Thank you. I have finished my project. Can you explain about maximum capabilities of log file in logo 8.fs4 |
5/25/2021 8:18 AM | |
Joined: 12/18/2014 Last visit: 7/21/2024 Posts: 33381 Rating: (4143)
|
If you mean the data log, then read the PDF in the attachment.
AttachmentLOGO! 8 manual 0BA8 2016_07 (FS4) pages 273+274.pdf (277 Downloads) |
Follow us on