5/14/2009 1:35 PM | |
Joined: 4/24/2006 Last visit: 6/18/2024 Posts: 8683 Rating: (1159) |
Dear Kaufic, The datarecords of Recipe are entered in OP and also stored on OP. When you transfer 1 record to CPU it will appear in DB31 starting at DBW0 and 12 words long. Here is manual of OP27: http://support.automation.siemens.com/WW/view/en/1142800 See chapter 9, to use Memory card to load or store Recipes. Best regards, Wizard |
5/14/2009 4:37 PM | |
Posts: 28 Rating: (0) |
Hi, so, all data are in flash memory ?Is not possibility this data replace in source code of ProTool ? Thank you Best Regards Kaufic |
Follow us on