11/3/2016 12:43 PM | |
Posts: 3 Rating: (0) |
thanks very much ¡¡ tomorrow i try to backup the project using one of the archives for compatibility thanks again ¡¡ |
8/28/2017 11:35 PM | |
Posts: 1 Rating: (0) |
Hello, i have the same problem, Could you solve the problem? thank you! |
5/27/2019 12:12 PM | |
Joined: 2/19/2018 Last visit: 4/28/2021 Posts: 6 Rating: (0) |
Hello I have project file from OEM. I try monitor to any block from that project to CPU but it have message "The program on the CPU is incompatible with STEP 7 project ( same attach file ) Can you solve the problem ? Best regards Yutthana AttachmentDoc1.pdf (291 Downloads) |
5/28/2019 11:40 AM | |
Joined: 2/19/2018 Last visit: 4/28/2021 Posts: 6 Rating: (0) |
Hello I can to mornitor success. I use TIA V13 SP1 and don't upgrade to project. Best regards Yutthana |
Follow us on