6/29/2021 10:20 AM | |
Joined: 5/6/2019 Last visit: 4/22/2024 Posts: 78 Rating: (0) |
Hallo, I have a little bit different problem. After installation of Profiletester with Proneta, the tool opens only with Network ananlysis. The rest of the icons and the page itself is different. I am attaching the screenshot of the page here. Also the trace.log says System:ArgumentOutof Range Exception.An excerpt from this is also attached. Has anyone faced a similar situation before. Jsut curious to know the source of problem itself. I am using Profiletester with Proneta and CP1616 driver. The software used to interact with CP1616 is TIA 15.1 Thanks, Bindu AttachmentProneta_Forum.pdf (76 Downloads) |
Follow us on