9/14/2009 10:52 AM | |
Joined: 12/2/2008 Last visit: 4/9/2024 Posts: 7 Rating: (3) |
A typical configuration to control hydraulic servo valves positioning controlled with T-CPUs(315T or 317T) looks like: |
9/15/2009 5:56 PM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326)
|
Sorry, I meant a position controlled hydraulic zylinder with a valve, just like the Jerkshowed in his posting. |
|
|
8/30/2013 6:34 PM | |
Posts: 2 Rating: (0) |
Here is a small program Siemens helped me with a while back. Change the max speed setting by moving a setting into DB88 Max speed and change position by moving a setting into the position set point. A simple move command will do the job just fine. Hope it helps, Curtis AttachmentHydraulic_Control.zip (406 Downloads) |
2/16/2020 4:16 PM | |
Posts: 3 Rating: (0) |
i have done this with S7-416 and FM458 |
Follow us on