5/29/2011 5:34 PM | |
Posts: 8946 Rating: (999) |
ProTool is canceled a long time ago... May be you will find some at ebay? |
5/29/2011 5:40 PM | |
Posts: 204 Rating: (1) |
|
5/29/2011 6:44 PM | |
Joined: 5/28/2009 Last visit: 6/28/2024 Posts: 127 Rating: (10) |
hi.......Nashwa_459 PC-------------OP7/17/27 2-RX-----------TX---4 3-TX-----------RX---3 5-GND----------GND-12 7-RTS----------CTS--5 8-CTS----------RTS-10 OP 27 cable |
Regards, |
|
This contribution was helpful to1 thankful Users |
5/29/2011 6:56 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, So - in practice you will need a Seriell RS232 (6XV1440-2K..) cable. And of course Protool - http://support.automation.siemens.com/WW/view/en/9560727 Contact with local Siemens rep. Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
6/1/2011 1:01 PM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating: (159) |
Hi Nashwa_459 Here is the link to the Manual In that 13.1.1, 16.4 & Interface Assignments B Page no.195 |
Ammy |
|
6/1/2011 5:37 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, So, Ayman already shew you the possible type of cables which are possible to use there. I want to mention a li nk where is possible to find pin's descriptions of different cables What connecting cables are there for connections between the operator panels and the different controllers? And you can't to use the MM KIT...as you will see. best regards, Hristo Mihalev |
Follow us on