7/20/2011 7:05 PM | |
Joined: 9/27/2006 Last visit: 4/27/2025 Posts: 12347 Rating:
|
Hello Tomy; Unfortunately a psb file is a Prosave extraction file, that is basically the compiled program finside the panel. You cannot open and modify it, only dowload it to the exact same panel number. Here is an extract from a very good FAQ that can help you understand the matter: "If you want a retransfer whose file can be edited, you must use the Retransfer function in ProTool or WinCC flexible. This is only possible with panels that support this function and in which retransfer is enabled in the transfer settings." FAQ:How do you backup/restore with a Windows-based panel? Also, follow this earlier discussion (amongst many others) on the same subject in the forum: Thread on psb file restore: /tf/WW/en/Posts/53955
|
This contribution was helpful to
1 thankful Users |
Follow us on