6/30/2024 10:35 AM | |
Joined: 9/9/2023 Last visit: 7/18/2024 Posts: 24 Rating: (0) |
Good morning, I use a program to vary the speed of a fan (controlled by an ATV12 altivar) using a PT1000 probe.this one works perfectly. I would like to add a command for a circuit breaker, once the machine door is opened the fan stops.once the door is closed the program resumes its normal course. I would also like to add a two speed switch.To be able to turn the fan once outside the program temperature ranges. I can't program these two functions.Can you help me? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 07/01/2024 13:08:41New subject after splitting |
|
6/30/2024 10:37 AM | |
Joined: 9/9/2023 Last visit: 7/18/2024 Posts: 24 Rating: (0) |
Here is the connection diagram
AttachmentRaccordement provisoire.pdf (193 Downloads) |
6/30/2024 3:12 PM | |
Joined: 12/18/2014 Last visit: 9/27/2024 Posts: 33843 Rating: (4206)
|
Please upload your LOGO! program as a ZIP file. |
7/2/2024 4:16 PM | |
Joined: 9/9/2023 Last visit: 7/18/2024 Posts: 24 Rating: (0) |
here is the program in ZIP file
AttachmentSchéma des connexions2.zip (170 Downloads) |
Follow us on