10/14/2016 7:37 AM | |
Joined: 1/21/2013 Last visit: 10/8/2024 Posts: 4620 Rating: (708) |
Hello William, The 224XP "6ES7 224-2BD23" like the one that our friend Lu has also it can be as MPI Slave or I'm wrong? 6ES7214-2BD23-0XB0 - Product Details - Industry Mall - Siemens WW |
10/14/2016 4:31 PM | |
Posts: 5225 Rating: (1192)
|
Hi. Yes it is possible to have the S7-200 link as MPI slave. That however does not make the port an MPI port.. it is a PPI port. There are differences between PPI and MPI. There are enough the same to make the S7-200 link as MPI slave. There enough differences to prevent having the S7-200 be an MPI master. w |
Follow us on