7/11/2013 5:18 PM | |
Joined: 1/28/2009 Last visit: 10/26/2024 Posts: 6852 Rating: (1365) |
That is possible with using 2 timers (on-delay and off delay) or counting clock pulses of CPU.Simulation of S7 1200 is not possible withoout the hardware .But you can try PLCSIM V12 and S7 1500 as starting point.Same issue here:
3s ON , 6s OFF timer |
Last edited by: hdhosseini at: 7/11/2013 5:19 PMLast edited by: hdhosseini at: 06/04/2019 18:51:50 |
|
This contribution was helpful to2 thankful Users |
7/11/2013 5:50 PM | |
Posts: 6 Rating: (0) |
thank you for the answers. |
Follow us on