5/13/2013 2:21 PM | |
Posts: 7 Rating:
|
is there anybody help me? |
5/13/2013 3:02 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating:
|
Hi, Unhappily I don’t have a “step by step” guide. However here there is the main steps and some print screens: 1 – Enable the PWM 2 – Set the PWM as you need. In this example, it runs in the scale 0..100 (Hundredths), with a time window of 100ms 3 – Check the configured addesses (in this case, Q0.0 is the physical output and QW1000 the virtual output) 4 – Build a logic moving values in the range (0..100) to QW1000. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\Pictures.zip (650 Downloads) |
Denilson Pegaia |
|
5/14/2013 11:40 AM | |
Joined: 8/1/2012 Last visit: 7/31/2024 Posts: 179 Rating:
|
[quote user="hrnn"]Hi i changed this settings but no change it doesn't work. Could you send sample project about PWM plz?. I suppose that use wrongly. How can i use it? Plz help me
see this
Attachmentpwm.zip (464 Downloads) |
|
|
This contribution was helpful to
1 thankful Users |
5/14/2013 12:41 PM | |
Posts: 7 Rating:
|
thanks for your replay ... I have CPU 1215c how can i change my device settings? I changed device but it had a error.
|
5/14/2013 1:47 PM | |
Posts: 7 Rating:
|
I did your advice but no change . you can look attachment. I cant see outputs led. |
Follow us on