5/25/2020 11:32 PM | |
Joined: 5/25/2020 Last visit: 8/2/2021 Posts: 1 Rating:
|
Hello! Please HELP! Have the same error with my PXC100ED:
The Firewall turned OFF, all configured, ping is OK, Node is configured... Even it was worked fine few days ago... I cant recognize the problem. I can see online parameters but can't download programs, or even see/edit parameters in "Online Properties. I tried reinstalling for all XWP programs and tools, tried "Run as administrator" for CFC. I also tried changes in "Communication Settings" and in "Set PG/PC interface" program. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_3663839 at: 05/25/2020 23:34:36Last edited by: AutoGen_3663839 at: 05/25/2020 23:37:00Last edited by: The Helping Hand at: 05/26/2020 12:54:41New subject after splitting |
|
Follow us on