6/10/2018 4:09 PM | |
Joined: 3/14/2008 Last visit: 5/21/2024 Posts: 2067 Rating: (928)
|
No! This is not correct... As of PCS7 V9.0 the CFC editor has a new feature. It detects automatically if the runtime sequence is correct. The vertical line means that the runtime sequence is not correct, or at least according to the editor... See attachement for info on this matter. And yes, it's a small section in the manual, it should have been somewhere under: "What's new".
|
Last edited by: Oreca at: 6/11/2018 8:48:08 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on