6/16/2009 7:58 AM | |
Joined: 9/28/2007 Last visit: 2/10/2022 Posts: 47 Rating:
|
Hi I have one question about COMPROFIBUS V5.1. I want to read IM308C program online. I use CP5511 to read. Step 1: The PC/PG Interface is CP5511(COM PROFIBUS). (picture 1) Step 2: I select the DP Master. (picture 2) Step 3: I select the IM308C address. (picture 3) Step 4: (picture 4)-->(picture 5)-->(picture 6) I very sure that I install software is OK. But,why I can not read on IM308C program? Attachmentcomprofibus V5.1.zip (76 Downloads) |
6/18/2009 3:27 AM | |
Joined: 10/7/2005 Last visit: 10/2/2023 Posts: 2989 Rating:
|
Hello fish please check the following: 1.) Do you also have Step7 installed on the OS where your COM PB is installed? If so, it could explain the problem you are having (the two clash with regards to the Set PG/PC interface). I always run Com Profibus from a seperatepartition (with its own Windows OS) to avoid conflicts between the "legacy" applications and the current Siemens programmign tools. 2.) What Windows OS are you using (i.e. if its XP you are out of luck)? Have a look at these two FAQ's for more info on compatibilty Compatibility of COM PROFIBUS versions with Windows operating systems Applicable PROFIBUS CPs for the application ONLINE-Functions in COM PROFIBUS I hope this helps Cheers Fritz |
Cheers |
|
6/18/2009 9:09 AM | |
Joined: 9/28/2007 Last visit: 2/10/2022 Posts: 47 Rating:
|
Now,I can read IM308C flash card program already. Thanks. |
Follow us on