11/29/2019 11:19 AM | |
Posts: 18 Rating: (0) |
Thank for reply! It's a lot more clear now. If I'd go with Basic KPT700 HMI instread, would a basic Step7 licence be sufficient for both (plc &hmi)? |
11/29/2019 11:27 AM | |
Posts: 1283 Rating: (105) |
WinCC Basic software license 6AV2100-0AA05-0AH5 WinCC is for Panels and SCADA and Step7 is for PLC programming. So two licenses are must |
This contribution was helpful to1 thankful Users |
12/3/2019 4:19 PM | |
Posts: 18 Rating: (0) |
I'm back with one more question. I found this: 6ES7822-0AA05-0YA5 - apparently it can be used for s7 1200 and BASIC HMI panels. Can anyone confirm it? |
12/4/2019 10:28 AM | |
Posts: 18 Rating: (0) |
So no need to buy 2 separate licences... why doesn't Sioemens make it more straitforward? ... Thanks |
6/29/2022 6:04 AM | |
Joined: 3/7/2022 Last visit: 6/26/2024 Posts: 4 Rating: (0) |
I think so step 7 basic is enough for HMI KTP 700 Basic check the datasheet attachment |
Follow us on