8/23/2017 12:32 PM | |
Joined: 1/15/2015 Last visit: 3/22/2022 Posts: 66 Rating:
|
Hello Friend , I made this sample project to test how the SINAMICS G110 works with USS protocol but it is not working , i changed the following parameters in the G110 as recommended , may anyone please tell me where is the problem . Thank you in advance. G110 configuration : USS Address= P2011 = 0 USS Baud Rate =P2010 = 6 = 9600 bps USS PZD Length =P2012 = 2= Two 16 bit words are in the Frequency Setpoint = P1000 = 5 =Frequency demand via USS protocol (HSW) Command Source= P0700 = 5= Via USS protocol (STW) Please download the PLC program (TIA V.11) from the following link : ---deleted Link, added file as an attachment-- AttachmentUSS test.zip (113 Downloads) |
Last edited by: Jen_Moderator at: 8/24/2017 1:26:26 PMAdded file as an attachment |
|
8/23/2017 3:02 PM | |
Joined: 1/30/2006 Last visit: 3/17/2025 Posts: 310 Rating:
|
Hi Have you tried this sample project https://support.industry.siemens.com/cs/us/en/view/40157517 It's an older version, but for the Drive everything shold be the same. in the S7-1200 you have to update. |
BR. Sven |
|
This contribution was helpful to
1 thankful Users |
Follow us on