5/14/2018 2:24 PM | |
Joined: 7/9/2015 Last visit: 10/15/2024 Posts: 3976 Rating: (593)
|
Hi, do you know the Entry: With which devices can the S7-1200 communicate via the integrated PROFINET interface and which protocols does the S7-1200 support?Regards, Towome |
|
|
5/14/2018 3:27 PM | |
Posts: 29 Rating: (0) |
Yes, thank you; My question Is : If I have more than 8 connection in my connection list ( for example 16 connections from ID to 101 to 116) and I want to use for example only 8 of these connections concurrently using GET requests, then switch to the other 8 connections , what can I do? My plc is a s7 1200, and ll the 16 s7 remote servers are always on; |
5/14/2018 3:28 PM | |
Posts: 29 Rating: (0) |
My doubt is also, if the connection enable and disable automatically when GET is enabled and disabled or not |
Follow us on