7/13/2023 4:17 PM | |
Joined: 12/18/2014 Last visit: 6/21/2024 Posts: 33216 Rating: (4110)
|
Attached is a sample project of how I would do it. You need to match the IP addresses of the two devices to your IP addresses. The Modbus access is enabled in the file properties of the LOGO!, the LOGO! is the client. AttachmentOne_bool_to_Modbus_device_8.3.zip (496 Downloads) |
7/17/2023 8:38 AM | |
Joined: 7/3/2023 Last visit: 8/8/2023 Posts: 11 Rating: (0) |
I updated now to 8.3.1 but it is still the same problem. |
7/17/2023 8:43 AM | |
Joined: 7/3/2023 Last visit: 8/8/2023 Posts: 11 Rating: (0) |
|
Follow us on