9/1/2009 1:47 PM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046) |
You did nothing wrongdear sko4in. This is merely a display "issue" in HWconfig which only disaplys "Entry 1" from the IM463-2 configuration, the IM will however work as configured. Have a look at the address overview (to be found in the "View"drop menu) and it will display correctly the whole configured address ranges of the IM463-2. I hope this helps P.S: Are you sure your S5 I/O's do "occupy"all the coonfigured IM463-2 addresses, or is this just a test configuration? |
Cheers |
|
9/1/2009 1:50 PM | |
Posts: 5 Rating: (0) |
Thank you for response! It is just a test, preparation for upcoming project so to say. Kind regards, Sergey |
Follow us on