4/25/2018 11:40 AM | |
Posts: 3 Rating:
|
Hi everybody, I want to ramp a pid in l/min is this possible |
4/25/2018 2:27 PM | |
Joined: 4/28/2015 Last visit: 5/2/2025 Posts: 398 Rating:
|
Hello, do you have more information about the controller you use and the application you want to realize...? |
5/3/2018 11:31 AM | |
Joined: 4/28/2015 Last visit: 5/2/2025 Posts: 398 Rating:
|
Hello, is 100% equal to 2l/min? |
5/3/2018 11:44 AM | |
Posts: 3 Rating:
|
yes but i don't know if the ramp is linair growth or exponential growth. |
5/3/2018 2:04 PM | |
Joined: 4/28/2015 Last visit: 5/2/2025 Posts: 398 Rating:
|
Hello, for getting the compensation characteristics of a valve manually, you could read the following FAQ: S7-1500(T): Manual determination of a compensation characteristic for hydraulic valves and hydraulic axes And for using this characteristics, you could read the following application example: Using the MC-PreServo and MC-PostServo organization blocks While using the FAQ and the application example, it is not necessary to use a PID control. For this, it is maybe possible, to use TO PositionAxis directly for controlling the valve... Maybe, it will help... - But I don't know, if it also works with S7-1200. |
Follow us on