6/22/2021 12:57 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello SummerSeaSun, the folder "C:\Program Files (x86)\Siemens\WinCC\aplib" of the installation Possible reason for this error: see the FAQs: https://support.industry.siemens.com/cs/ww/en/view/868014 "With WinCC V7.5 and higher or WinCC Professional V16 and higher how do you activate the setting https://support.industry.siemens.com/cs/ww/en/view/109769234
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
6/22/2021 1:38 PM | |
Joined: 2/5/2013 Last visit: 3/26/2024 Posts: 287 Rating:
|
Thank you for the answer, it's not the case, no network is involved here, I've made some edit, removing this row, fix the error:
I've moved this function to the PDL that is loaded in the Picture Window PopUP. Now I assume this is the best practice: - set tag prefix from MAIN_PAGE - read tag prefix from inside of POPUP.PDL that will be dynamically loaded from the MAIN_PAGE Is this correct? |
Follow us on