1/12/2022 4:50 PM | |
Joined: 5/30/2014 Last visit: 6/27/2024 Posts: 146 Rating: (18) |
I have found a solution for my problem. So, if RCV_PTP returns an OK code (16#0099) but zero LENGTH, I use these conditions to iterate loop call to RCV_PTP until it returns OK code and non-zero LENGTH. It works with only one iteration after zero LENGTH. See the explanation of this behavior in the next post! |
Last edited by: C-3PO at: 06/22/2022 16:03:47Wrong conclusio deleted If you find my contribution helpful please RATE it :)) |
|
This contribution was helpful to1 thankful Users |
6/22/2022 3:59 PM | |
Joined: 5/30/2014 Last visit: 6/27/2024 Posts: 146 Rating: (18) |
After thorough researching, I have found the answer for my problem. It is described in documentation (System Manual, V4.4 11/2019) on page 1194: When the EN_R input is TRUE and a message is available, the CPU transfers the message
So, I did not enabled EN_R and it was the reason the LENGTH was 0. |
Last edited by: Jen_Moderator at: 06/23/2022 09:00:51Link optimized. If you find my contribution helpful please RATE it :)) |
|
This contribution was helpful to1 thankful Users |
Follow us on