2/18/2013 1:00 PM | |
Joined: 3/21/2006 Last visit: 12/2/2024 Posts: 10229 Rating: (1181) |
No, it is not available. Here you can find almost the same discussion -Read SN or MAC address from PLC program |
2/18/2013 1:38 PM | |
Joined: 5/3/2012 Last visit: 6/23/2024 Posts: 161 Rating: (2) |
I am working with s7-300, with this cpu Ican´tread ip in any away. Thank you. |
7/2/2018 4:24 PM | |
Joined: 7/25/2015 Last visit: 6/13/2023 Posts: 2 Rating: (0) |
You can read the IP from the system record with RDREC. This is described in: FAQ,Entry ID:82947835,Entry date:04/29/2014 |
Follow us on