4/30/2019 5:12 PM | |
Posts: 12 Rating: (0) |
Hello Thanks for the reply. It's hard to find any decent information from Moxa. I added my configuration and the QModMaster in attachement to give some information. The values I need correspondent with a detection on the wire, short circuit, NO contact close, NC contact closed, both closed. That's it. I think the value I get from the Moxa is float. greetings, AttachmentLogo.zip (396 Downloads) |
5/2/2019 1:39 PM | |
Joined: 12/18/2014 Last visit: 8/30/2024 Posts: 33647 Rating: (4182)
|
Please upload your LOGO! program as a ZIP file. |
5/2/2019 2:14 PM | |
Posts: 12 Rating: (0) |
It's still something small, haven't started with the actual program because I wanted to get the correct value first. The NAI part is something I do get from the Moxa module, I tried filtering it so I get something that looks like my value. But I'm not satisfied with it. I need to get the value of the resistor, which is steady but it keeps differing in my program between 2 values. AttachmentTestProject.zip (443 Downloads) |
Follow us on