3/13/2015 9:48 PM | |
Posts: 4 Rating: (0) |
I have been trying to do the same. I am trying to communicate with a Modicom PLC and trying to read %MW1 and %MW2 registers in the PLC using Modbus/TCP port. I have no problems with the connection between WinCC and PLC, but I can't not get the values in the adresses %MW1 and %MW2. I don't know why, I think is something related with the addressing in WinCC in the holding registesr. (I have puted 3x400001 for %MW1 and 3x400002 for %MW2 without any success). It reads some value, but It's not the right value. Also I have changed the values in %MW1 and %MW2 and they doesn't change at all in WinCC, so the addressing is not right. Some advice please. Thanks
|
Last edited by: Min_Moderator at: 3/16/2015 11:13:32 AMNew subject after splitting Last edited by: Min_Moderator at: 3/16/2015 11:15:10 AMAdd quote |
|
Follow us on