7/2/2020 4:40 PM | |
Posts: 2 Rating: (0) |
Thank you for your quick feedback. Well, I am a developper and i would like to know where should I put the acyclic variables. in the DAP module? or in each module I affect it's acyclic variables? Because if I affect all acyclic variables in the DAP module, that's fine because we can find all acyclic variables in the DAP. But what I know is that the DAP module, we must insert only variables and parameters which are dedicated to the Ethernet protocol. If I want to affect the acyclic variables for each module, I need to drag and drop each module to the Device module structure to have its ow ID material. But what will happen if I don't do the drag and drop module? Regards, SaidSee attached pictures AttachmentDevice_Structure_View.zip (67 Downloads) |
Follow us on