Industry Online Support
Technical Forum
2/7/2012 4:27 PM | |
Posts: 1 Rating: (0) |
Hi, I'm trying to follow through this part of the help section. However, I can't seem to monitor MW70 "Out_Addr_1" in the VAT. When monitoring the OB1 containing the code, I can see the values changing though. Can someone point out what I'm missing? See attached image & video. Thanks a lot for helping out! Hmmm, will try to attach files later. Wmv file seems not allowed. PS. 1. How can I add jpg to show inline? 2. Is it possible to attach a 2nd file (zipped wmv)? |
Last edited by: Lexje at: 2/7/2012 8:30 PMLast edited by: Lexje at: 2/7/2012 8:28 PMAttached converted PNG to JPG file |
|
2/7/2012 6:10 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, You can zip your files, or make printscreens(jpeg, pdf) Mw/Md can be monitored directly PQW not (that is without some tricks) Here is a link to a thread where you can read more /tf/WW/en/Posts/62858 Regards, Marcjan |
Last edited by: Marcjan at: 2/7/2012 7:04 PMProblem solved? |
|
Follow us on