3/16/2020 1:18 PM | |
Joined: 2/22/2008 Last visit: 5/26/2024 Posts: 2698 Rating: (207) |
If you are also interested on tinkerer models, they also may be good, then look here You find these sensors at several dealers for low prices, but i have not checked for appropriate resolution, accuracy and output voltage/current for the Logo controller. First have a look to the data sheets or only by one test model. If you need several sensors, it might be possible to mount them in a case with terminals to save much money. Up to now if have no experience with these sensors. Regard, Scorp |
Follow us on