10/28/2011 6:08 PM | |
Posts: 111 Rating: (0) |
Hi all,
I am involved in a big project inside a gas station, to carry out my project, i need to read some other data from devices that previusely had been connected to other controllers. For example, as I attached the file, i have a transmitter that has been connected to a PLC and due to some reasons, I also need to have data of this device in my program. Can I connect signal from this transmitter to two PLCs at the same time? I have this problem with digital inputs too, how can I overcome this problem? i have mentioned the distance between each device. Regards AttachmentPlan.pdf (59 Downloads) |
10/29/2011 11:02 PM | |
Posts: 111 Rating: (0) |
Hi Can anyone help me pls?
|
Follow us on