Industry Online Support
Technical Forum
10/8/2008 1:54 PM | |
Posts: 487 Rating: (36) |
Hi Here is an example from what we use in a on mouse down vb script .I did delete or change some stuff that are not relevant or private. the trick is to create internal tags of the right kind and then call a "select" and extract the right stuff from the dataset You should be able to adept it to your situation Greetings Eric Attachmentcomplete external SQL for forum.zip (96 Downloads) |
Last edited by: aikona at: 10/8/2008 1:56 PM |
|
10/8/2008 2:00 PM | |
Posts: 487 Rating: (45) |
Yes, this is very much possible with VBS. Check the FAQ below for an example. http://support.automation.siemens.com/WW/view/en/16514261 You can also find come info in WinCC Information system under "Working with WinCC > VBS to create Procedures and Actions > Examples of VBScript > General examples". |
Last edited by: JMJ at: 10/8/2008 2:00 PM |
|
10/14/2008 2:24 PM | |
Posts: 6 Rating: (0) |
Hi Eric thanks, I'll try that. Greetings Roger |
Follow us on