Industry Online Support
Technical Forum
9/28/2012 3:21 PM | |
Joined: 9/27/2006 Last visit: 8/14/2024 Posts: 12277 Rating:
|
Hello h2; Simply put, you can read the HART variables from the HWConfig settings for the HART module.PDM is required to calibrate the HART field devices, and to integrate nw field devices in the hardware configuration. Here is a quote that should clear things up a bit: Configuration of HART variables You assign the HART variables in STEP 7 HW Config. You can configure up to 4 HART variables for a channel ● PV (Primary Variable) ● SV (Secondary Variable) ● TV (Tertiary Variable) ● QV (Quaternary) From the SIMATIC ET 200M distributed I/O device HART analog modulesmanual, Chapter 3: Instructions for configuration, commissioning and operation Here are a few more links that could give you more information: S7-300 I/O Analog -- Setting up and parameterizing hardware -- Information to HART modules and signals How are HART field devices installed in the HW Config? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/28/2012 3:22 PM |
|
11/11/2013 9:41 AM | |
Joined: 4/24/2009 Last visit: 8/2/2024 Posts: 2682 Rating:
|
New question splitted to start, stop, hold, reset totalizer Best regards O_Moderator |
Follow us on