4/7/2006 8:39 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (316) |
Hi guys, I have found a new link over Wireless Equipment, maybe this will bring you more information. [;)] IWLAN: Setup of a Wireless LAN in the Industrial Environment http://support.automation.siemens.com/WW/view/en/22681042 Best regards, Late |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
4/7/2006 12:33 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
In the acces point you can set the client module on Critical Compliant (CC). Now it is on Non Critical Satisfied (NCR), we already have in IFeatures >iQos resereved bandwith (500 kb) for the client moduleand theResponse time is 15 ms,howcan you get it on that Critical Compilant? Critical Compliant (CC) Critical Non-Compliant (CNC) Non-Critical Satisfied (NCS) Non-Critical Non-Responsive (NCNR) How low can the update time in the Hardware configuration be set, when the wireless communication is on Critical Compilant? |
Best regards, |
|
Follow us on