5/15/2012 2:20 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating:
|
Hi The Status code of 08A0 satnds for: There is no free receive buffer available:No receive buffer space available for receiving data. Corrective action is :The P_RCV FB must be called more frequently. Please use the sample code which you can download fromhere. In this sample code inside FC11 there is a provision for sending two request of different data length from different area of a DB. Already programmed. And if required you can increase it further. Please see below
|
This contribution was helpful to
1 thankful Users |
Follow us on