11/6/2020 9:42 AM | |
Joined: 2/9/2018 Last visit: 5/9/2024 Posts: 6 Rating: (0) |
I salute you all, The issue I encounter is described bellow: I created a recipe with desired name. I added the desired recipe elements and linked each element to the desired Tag. Then I created data records with desired name and added desired values to each record element. When I download the software to the HMI or simulate the HMI in TIA Portal, the displayed names for the Recipe, Data records, Data record elements is not the one I set in the project. Note: The data record elements values are loaded and displayed correctly. The issue is only with the Display Name of the elements, records, recipe. Software used : TIA Portal V13 SP2 Professional. Hardware used: KTP600 Basic Mono PN What could cause this issue? I do not receive any compile errors. See pictures to better understand the issue. [snip] AttachmentImages.zip (32 Downloads) |
Last edited by: Jen_Moderator at: 11/06/2020 12:17:37Removed links and added files as an attachment. |
|
11/6/2020 11:10 AM | |
Joined: 4/24/2006 Last visit: 6/3/2024 Posts: 8665 Rating: (1154) |
Hello, You have the column 'Display name', that is shown on the HMI panel. Best regards, Wizard |
Follow us on