3/31/2020 11:52 AM | |
Joined: 4/18/2014 Last visit: 10/4/2024 Posts: 253 Rating: (5) |
Hi experts, With reference to the attached manual am trying to simulate the recipe synchronisation from Main panel HMI to remote panel HMI. In DB i can exchange only the ingredients values and i can't exchange the recipe number and data record number to remote HMI DB. I checked logics and settings every thing is correct , so now my doubt is whether i can check this via simulation or not ? If i have real HMI means then it should work right? Thanks in advance. Attachment109736272_DOKU_v10_en.pdf (43 Downloads) |
Follow us on