11/18/2015 7:53 PM | |
Posts: 1 Rating: (0) |
Não consigo fazer com que o sistema reconheça o cabo USB/PPI para comunicar meu CLP S7-200 no W7 64bit. Alguém sabe se somente com um drivers eu conseguirei a comunicação ou só comprando um cabo novo? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/19/2015 11:33:47 AMNew subject after splitting |
|
4/26/2016 7:00 PM | |
Joined: 9/27/2006 Last visit: 5/20/2024 Posts: 12257 Rating: (2668) |
Hello wtjota; What version of S7-Microwin do you have installed on your programming PC? As you can see in the following attachment, only SP9 supports Win 7, 32- or 64-bits, and Win 7 drivers will only be installed with that version. If required, follow this link to download the SP 9: STEP7 MicroWIN V4.0 SP8 and SP9 https://support.industry.siemens.com/cs/ww/en/view/58523240 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/26/2016 7:08:26 PM |
|
Follow us on