2/15/2021 9:58 AM | |
Joined: 10/16/2020 Last visit: 7/11/2022 Posts: 1 Rating:
|
miami
And If I have a 1513 PRO do you have any suggestion for a SSI encoder converter ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/15/2021 13:48:43New subject after splitting |
|
2/15/2021 3:39 PM | |
Joined: 9/27/2006 Last visit: 4/19/2025 Posts: 12346 Rating:
|
Hello; The original solution proposed by Miami was to use a ET 200SP positionimg module, TM PosInput1, on a Profibus IM 155-6DP. to read the SSI interface of the encoder and transmit it to the controller over Profibus.
The CPU 1513Pro--2PN comes with 2 Profinet interfaces, one with a RJ45 connector, so a connection to a Profinet module can be quite simple. Have a look at this Product Note: https://support.industry.siemens.com/cs/ch/en/view/109771704 A ET 200SP module (such as the recommended TM PosInput 1) can operate on a Profinet network if you select a Profinet IM, IM 155-6 PN __ as you can see in this document: https://support.industry.siemens.com/cs/ch/en/view/99683390 The same positioning module could be operated with your S7-1513Pro-2PN, so the same solution could apply. Have a look at these pages from the TM PosInput1 manual: https://support.industry.siemens.com/cs/ww/en/view/109780353/132722229643 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 02/15/2021 15:40:46Last edited by: dchartier at: 02/15/2021 15:48:34 |
|
Follow us on