Industry Online Support
Technical Forum
9/15/2010 1:59 PM | ||||||
Posts: 3609 Rating: (29) |
Import of a Technical Question of an User boopathi@sequent wrote: Dear All, below mentioned Rdundancy bundle for im153-2 selection information
|
|||||
9/15/2010 2:56 PM | |||||
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating: (2675) |
Hello boopathi; For every pair of I/O modules (40 mm wide, which is the standard), you will need the following bus module:
However, just take care that the IM 153-2 can only support 12 I/O modules on the rack, and that you say you are planning to use 16, am I right? See the description of your IM 153-2 (from the Industry Mall):
You will need to split the I/O modules over 2 racks in that case, which means 2 IM 153-2red-bundles... Hope this helps, Daniel Chartier |
||||
Last edited by: dchartier at: 9/15/2010 4:10 PM |
|||||
This contribution was helpful to1 thankful Users |
10/4/2010 8:35 AM | |
Posts: 79 Rating: (0) |
thanks i got clear idea. |
Follow us on