9/10/2019 3:36 PM | |
Joined: 9/27/2006 Last visit: 12/1/2023 Posts: 12180 Rating:
|
Hello Kashir; It appears the features you are looking for are part of the S7-400H systems, and are not yet available in the S7-1500 RH PLCs. See this presentation of the S7-1500 RH system: Compare with this manual for the S7-400H, especially the section Using I/Os in the S7-400H: SIMATIC Fault-tolerant systems S7-400H (V6.0) https://support.industry.siemens.com/cs/ww/en/view/82478488 And this document shows the use of MTAs (Marshalled terminaltion assemblies) with the S7-400H (I do not remember having seens any MTA for the S7-1500 family): Configuration of Redundant I/O Modules in SIMATIC PCS 7 https://support.industry.siemens.com/cs/ww/en/view/28430682 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/10/2019 15:43:47 |
|
This contribution was helpful to
1 thankful Users |
Follow us on