9/23/2008 2:13 PM | |
Posts: 487 Rating:
|
If you use 400H, redconnect is the best option to have and yes, it is a must to use Siemens ethernet cards. Redconnect configuration is not supported on generic NICs. Kepware has some options by keeping two OPC servers on two different PCs or even 2 virtual PCs and then using redundant master option from kepware. Check the link below http://www.kepware.com/KEP_KB/default.asp?ToDo=view&questId=324&catId=99 |
9/23/2008 8:50 PM | |
Posts: 487 Rating:
|
|
Last edited by: JMJ at: 9/23/2008 8:51 PMOops! Forgot to attach JPEG |
|
Follow us on