12/8/2023 9:07 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello Koen1971, From your discussion so far, I guess your 2nd measuring system is defined as active measurement feedback & of incremental liner scale with distance coded reference marks at interval of 20 mm. So disconnection of motor & reassembly is not going to affect referencing of axis any way. In system data & PLC logic axis referencing is configured as move axis either in +ve or -ve direction & when axis travel hit the reference mark of 2nd measurement system, which is active, axis gets referenced & accordingly co-ordinate value is displayed. Hope this helps. |
This contribution was helpful to
2 thankful Users |
Follow us on