9/30/2016 1:26 PM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
WinCC V14 TRIAL https://support.industry.siemens.com/cs/ww/en/view/109740228 |
This contribution was helpful to
5 thankful Users |
9/30/2016 4:43 PM | |
Posts: 2 Rating:
|
No support for Windows 10 until SP1. |
9/30/2016 5:02 PM | |
Posts: 5225 Rating:
|
Hi. I am working through the document... My focus is on the changes made for the SCL coding .. it is an impressive set of additions. Several additions cover requests and struggles that appeared on this Forum. Some of the additions are even things that I would have liked to have, but did not even bother to enquire about. It seems on paper at least, a good version to upgrade to. One caution though.... there is no such thing as a compatibility mode. You can not have a TIA V13 SP1 file open in TIA V14 without converting first. So you'll have to keep a copy of TIA13 active when you have older projects that you want to keep from upgrading to TIA14. w Update: |
Last edited by: William_B at: 10/1/2016 4:25:45 PMErronous statement marked with strike-through. Add update note. |
|
This contribution was helpful to
6 thankful Users |
10/1/2016 11:06 AM | |
Posts: 24 Rating:
|
Startdrive link not working W10 is out for more over a year now and still no Tia support? Requirements on RAM totally sick |
10/5/2016 12:22 PM | |
Joined: 8/14/2014 Last visit: 4/5/2024 Posts: 144 Rating:
|
By accident low requirements are fulfilled by basic version of SIMATIC Field PG M5, and high by advanced |
10/5/2016 1:37 PM | |
Joined: 3/14/2016 Last visit: 9/1/2024 Posts: 162 Rating:
|
So as I can see the Optional Package - i.e. Starter integrated on TIA Portal - is not available yet, I hope, for V14. Is that correct? |
"Engineers like to solve problems. If there are no problems handily available, they will create their own problems." (Scott Adams) |
|
10/5/2016 1:47 PM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
what do you mean exactly? STARTER is no SW Package for TIA, is a Classic Prouct. So what you mean exactly with the Starter integrated on TIA? |
This contribution was helpful to
1 thankful Users |
10/5/2016 1:51 PM | |
Joined: 3/14/2016 Last visit: 9/1/2024 Posts: 162 Rating:
|
I ment SINAMICS Startdrive. Now I saw the note:
|
"Engineers like to solve problems. If there are no problems handily available, they will create their own problems." (Scott Adams) |
|
Follow us on