10/16/2007 11:22 AM | |
Posts: 5822 Rating:
|
Hello, well there are two things to care about. First of all: Have you read this FAQ? How do you implement communication with TeleService S7 via a mobile phone? Secondly: Sadly is the use of the TC65 not allowed with the TS Adaptor II. If you use a TS Adaptor IE you may use the TC65. There are special Initialization Strings to use, but sadly is this FAQ only in German available. Warum kann das TC65T nicht mit dem TS Adapter II eingesetzt werden? Best regards J_Bell |
10/16/2007 1:03 PM | |
Posts: 28 Rating:
|
Hello, This is not so goof information for us but very useful Attachmenttc65t_hw_interface_description.pdf (293 Downloads) |
Follow us on