2/25/2022 11:39 AM | |
Joined: 7/4/2021 Last visit: 5/24/2022 Posts: 6 Rating: (0) |
Configuration tia portal |
3/7/2022 2:26 PM | |
Joined: 8/3/2009 Last visit: 6/10/2024 Posts: 12991 Rating: (1659) |
Hello SimoRouini Try using the IP address of the PLC instead of name. Use the basic binary tcp notation: opc.tcp://IP-address:Port Do you have created a Server interface for the OPC UA Server in S71200? Check also in the example: https://support.industry.siemens.com/cs/de/en/view/109737901 Bye Murof |
Last edited by: Murof at: 03/07/2022 14:27:00Last edited by: Murof at: 03/07/2022 14:27:38If this Information really helps, you could use the Rate function |
|
Follow us on