8/31/2024 1:17 AM | |
Joined: 8/31/2024 Last visit: 9/17/2024 Posts: 1 Rating: (0) |
Para reemplazar estos bloques BGN y CALL en el Tia Portal para un S7 1200. Que serian los temporizadores RT y PT? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/02/2024 08:19:25New subject after splitting |
|
9/2/2024 5:48 AM | |
Joined: 3/30/2020 Last visit: 10/13/2024 Posts: 4858 Rating: (993)
|
A more exact answer is only possible if you show us some code. A screen capture would be most welcome. The BGN_ITIME and CAL_ITIME (calculate) was meant to be used as software timers. In the S7-1200 we have the IEC-Timers. Perhaps the following FAQ will be helpful to see if your application needs a TON / TOF / TONR / TP type timer |
Last edited by: Moderator_Lan at: 09/02/2024 08:17:13link optimized Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on