1/22/2016 2:39 PM | |
Posts: 13 Rating: (0) |
Thank you for sincere help and brief explanation. That was so nice of you . I shall try it out and inform you if I found any problem |
2/9/2016 2:44 PM | |
Posts: 13 Rating: (0) |
Dear Sir Enclosed please find attachment Now I have to replace the 750-303 with ago 750-333 bus coupler. I have already installed gsd.exe file and can see all the modules in the standard catalogue. I have drag the 750-333 FW 03 in the first slot and Now as per attachment which modules I need to add? These were the previous already installed I/O modules with 750-303 Which Parameters assignment I need to change? I have to change the profibus node address also as per the pin on module Please advice Best Regards, Qasim Attachment8 di wago.pdf (143 Downloads) |
2/11/2016 8:14 AM | |
Posts: 13 Rating: (0) |
Dear Sir, Thanks for your support. We have a client who has 750-303 No. is 34010502---B030303 and is replacing with 750-333 Firmware loader is 03. Do I need to replace the I/O, and relay also or only the field bus coupler will be sufficient as I can only put modules from 730-333 standard catalogue and the older 750-303 Fw 02 is not available in catalogue ? Would the 750-303 modules be compatible with 750-333 bus coupler? The older Modules installed with 750-303 are as under 750-602 supply input = 2 750-554 analog output =12 750-400 digital input = 4 X 2 =8 750-517 relay output = 28 750-600 end terminal = 1 And in the Simatic manager its shown in attachment. Also I can't find 750-600 end terminal in 750-333 modules. What is the replacement for this? Please provide step by step procedure.
I shall be thankful for your support
Best regards, Attachment8 di wago.pdf (121 Downloads) |
Follow us on