2/10/2016 10:20 AM | |
Posts: 13 Rating: (0) |
Dear Sir I hope you are doing great. Enclosed please find attachment Sir, I have to replace the 750-303 with ago 750-333 bus coupler. I have already installed gsd.exe file and can see all the modules in the standard catalogue. I have drag the 750-333 FW 03 in the first slot and Now as per attachment which modules I need to add? These were the previous already installed I/O modules with 750-303 Which Parameters assignment and configurations I need to change? I have changed the profibus node address also as per the pin on module. I have also put the I/O addresses as per attachment. Please advice I shall be thankful for your support and services
Best Regards, Qasim ------------------------------------------------------------------------------------------ Attachment8 di wago.pdf (167 Downloads) |
Last edited by: Min_Moderator at: 2/10/2016 3:22:03 PMNew subject after splitting |
|
Follow us on